This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: Solution for LiHV 9S pack

Part Number: BQ76930

Tool/software:

Hi TI team,

I am searching for a simple solution to protect two 9S battery packs composed of cells whose voltage range must strictly be kept within the range of 3.4V - 4.5V and 3V - 4.25V respectively, and I would like to use the same PCB for both. It would be much appreciated if you could recommend me a solution that can perform at least voltage and temperature protection for both. A balancing function would also be appreciated. Ideally, the solution would not require programming, but I know that with these unique requirements, it is probably a necessity, and that is ok.

Thank you so much.