Tool/software:
At startup, the resonant burst waveform goes wrong.
The Vcr waveforms are shown in Figures 1 and 2.
Normally, Vcr detects a shunted resonant current, but it rises to 7V despite the fact that no resonant current is flowing.
Why is this behavior occurring?
Also, how do I resolve this issue?
Requirement
Iout=0A
Vout=24V