This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131: Inductor Spec Confirmation

Part Number: TPS65131

Tool/software:

Hi

May I ask if there is any current (Imax) limit for the L8/L9 4.7uH parts in this +/- 12V circuit diagram?

Because I need to replace the TDK 4.7uH with Zenithtek 4.7uH (common material) parts, thank you.

Currently using TDK 4.7uH spec

Replace with the following alternatives.