Other Parts Discussed in Thread: TLV61047
Tool/software:
Hi,
I am designing Boost regulator using LM2698 with following specs
Vin = 5.2V
Vout = 11.6V
Iout = 0.4A
L = 10uH
Fsw = 1.2MHz
Power stage calculation
Dominant Pole Freq : 248Hz
RHP zero Freq : 92KHz
ESR zero freq : 724KHz
- My R and C compensation values are Rc = 40K and Cc= 1nF
- which give compensation pole at 182 Hz and compensation zero at 4K.
Can you please confirm if my system will be stable with the calculated values ?
Regards,
Anurag Singh