Other Parts Discussed in Thread: LMG1020
Tool/software:
I am testing a pulsed laser diode (SCW 1637-250R) using TI LMG1020EVM driver board to generate short pulse width for laser diode.
I put this laser diode on LMG1020EVM board and applied Vbus from 1V and increased this voltage slowly up to 12V. But I don’t see any voltage changes at Cathode node of laser diode and also current changes (0A) from the DC power supply generator for Vbus voltage (The max current limit in power supply generator is set to 1A for Vbus voltage).
Since this laser diode operating 1625nm of wavelength, we used ThorLabs VIS/IR Detector card to see the laser light visually, but no light is shown in the Detector card.
The input signal to the gate of GaN FET (EPC2019) inside of LMG1020 chip has 5.5V, 20n sec of pulse width, 1u sec of repetition rate.
Can you know how I can make this SCW 1637-250R laser diode operate with TI LMG1020EVM board?
Here are some images from our test setup.
1. LMG1020 EVM board with SCW 1637-250R - Anode and Cathode are connected as LMG1020EVM manual suggested.


2. Yellow waveform: Input signal from arbitrary signal generator to LMG1020EVM board
Green waveform: IN+ voltage on LMG1020 (5.5V, 20n sec of pulse width, 1u sec of repetition rate)
Blue waveform: Vg on LMG1020EVM (gate voltage to GaN FET of LMG1020)
(please ignore the red waveform)