This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2547: Regarding the difference in iPhone behavior between SDP1 and DCP on TPS2547.

Part Number: TPS2547


Tool/software:

Hi AE,

       Currently, The Type-C port with BC1.2 via TPS2547 and the CC pins handled by a CC controller for Type-C protocol.

       We support 5V3A

       Current testing on the iPhone 15 shows different results between DCP and SDP1 as follows.

       1.  If both SDP1 and DCP are present with DM/DP and CC1/CC2 connected, which protocol will iPhone 15 follow?

       2.  When the phone is in DCP mode, it intermittently stops charging, and a PD hard reset is observed.

Best Regards

  • Hi Bruce,

       1.  If both SDP1 and DCP are present with DM/DP and CC1/CC2 connected, which protocol will iPhone 15 follow?

    I do not know, for BC1.2, the device (the Iphone in this case) drives the detection, so it is up to it to determine which protocol to follow. I would assume it would attempt the higher power one (DCP), but cannot say for sure as it is up to the Iphone to decide.

    2.  When the phone is in DCP mode, it intermittently stops charging, and a PD hard reset is observed.

    Do you see the voltage drop or current surge? I'm assuming the fault pin goes low?

    Thanks and Regards,

    Chris