Other Parts Discussed in Thread: TIDA-010208, , EV2400,
Tool/software:
Hi Guys,
I'm attaching a schematic for a standalone design - 4S Schematic
The schematic is based on BQ76922EVM and TIDA-010208. Kindly go through and suggest if any changes are recommended
1. I've disabled the internal LDO by connecting REG1 to VSS. Should I enable it and provide 3.3V pull-up for the I2C lines ? (I'm hoping that the EV2400 will provide the pull-up, for OTP)
2. I've used 10M resistors for PCHG and PDSG gate (R9, R10) - Is 1M recommended ?
Thanks & Regards,
Muki