Tool/software:
Hi all,
8.2.3.2 I have a question about Detailed Design Procedure.
How should I apply Vin and Vout for Cases A-D?
Vin=24 V (Max25 V) is supplied to LM5060. The voltage range varies in the range of 0~25 V. In this case, if Vin=0 V, Rsmin=0 Ω from (17).
Should I set the input to 0V and output to 24V?
I also checked the following calculation tool.
SLVC667 Calculation tool | TI.com
Minimum Input Operating Voltage: VIN(MIN)
Maximum Input Operating Voltage: VIN(MAX)
The values of recommended operating conditions are listed in each. 5.5V to 65V
Should I refer to this?
Best Regards,
Ryusuke