This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS16630-32EVM: TPS16630 is failing during the surge test (1KV)

Part Number: TPS16630-32EVM
Other Parts Discussed in Thread: TPS2663, TPS1663

Tool/software:

around

Hello Team,

We are using TPS16630 , e fuse as protection element in our 48V system .  We have used a TVS diode (SMBJ54A) which has working voltage of 54V and clamping voltage around 60V.

TPS16630 is set for over-voltage protection around 57V

During our surge test , we found that TPS16630 , over-voltage protection is triggering (response time is in uSec ? ) before TVS diode clamps to protect during the surge tests.

We are not able to find TVS diode with lesser clamping voltage (below 56V) while working voltage above 52V  (too narrow requirements )

Do you have any suggestions for this ?

Our operating voltage is 48V , needs to have over-voltage protection around 54V  and circuit needs to pass surge test as per IEC 61000-4-5

Please suggest.

thanks

Vasu