This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2005: version with interlock protection

Part Number: LM2005
Other Parts Discussed in Thread: UCC27710, UCC27282

Tool/software:

Hello,

Is there a version of LM2005 with interlock / shoot-through protection?

Thank you, Keith

  • Hi Keith,

    There is not a version of the LM2005 with interlock or shoot-through protection. However, the UCC27710 is a driver with the same pinout and interlock. However, it does not have an internal bootstrap diode. 

    Another option is the UCC27282. The UCC27282 has multiple package and pinout options, as well as 5V UVLO. 

    Best,

    Amy