Tool/software:
Hello,
I have used UCC27712 as full bridge driver circuit with external transistors that are based on PWM switching.
I am currently looking for a solution to drive the brushed DC motor with same setup, but different would-be DC or discrete signal (100% duty cycle) to drive the motor.
So the construction would be two of gate driver IC and 4 transistors which forms a full-bridge configuration. I want to be able to provide input as DC signal to switch transistors accordingly to provide power to the DC motor. Motor will be either running as forward or reverse direction depending on the input signals.
Is it something possible with UCC27712? I am seeing something in the datasheet mentioning about using as a separate bias supply and could work for 100% duty cycle but I wanted to clarify with the community and how this works.
Thanks