Other Parts Discussed in Thread: TPS272C45
Tool/software:
We control a linear motor. It takes about 2 A and can go in or out by reversing +24 V and GND. The relay switches the polarity. The software always switches the relay before turning on the HSS.
We have had two HSS blow up on power on. The 24 V comes from a 100 W ac to dc power supply that we have used for years on this product.
The chip seems to blow up as soon as the 24 V is present or it is ramping up. Because once we turn on the ac, the chip explodes within less than a second. The processor controlling the HSS is held at reset for 2½ s after the 24 V is present, so it has not yet controlled the HSS. The 5 V for the processor is derived from the 24 V.
We test the boards on the bench before putting it into the machine.
We can swap a board that has blown up with another identical board and it will work fine. But it's not every time that the boards will blow up.
What could be causing the chips to blow up?