Tool/software:
Dear team,
Would I know why 100mA IF diode is recommended to resistor-diode ground network? I understand the current only flows through Dgnd when normal operation, which means not reverse or power/gnd loss situation...
I see 10mA_max is the Inom shown below. If this is the one which only should be considered, then 100mA is too much.


I already read some apps notes below, but still not clear.
https://www.ti.com/lit/an/slvaes9a/slvaes9a.pdf
https://www.ti.com/lit/an/slvae30e/slvae30e.pdf
https://www.ti.com/lit/an/slvae55/slvae55.pdf
Best regards,
Yuto Kitamura