This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65219: TPS65219 BUCK1 Converter Switching Frequency

Part Number: TPS65219


Tool/software:

Hello,

Could you please explain Switching Frequency?

Under the following conditions, the switching frequency was evaluated to be 2.02MHz. Given that the voltage is correctly output, I believe there are no issues. What do you think?

BUCK1 Converter

Forced PWM
High Bandwidth Case
Forced PWM, VIN = 5.5V
VOUT = 0.85V
IOUT = 0A
Ta = 60℃

Thank you!