This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCP020509: Parallel connection on DCP020509 and current sharing

Part Number: DCP020509
Other Parts Discussed in Thread: UCC29002

Tool/software:

Hello,

In my application, I need to use 2 DCP020509 in parallel because I require a maximum of approximately 350mA of current.

According to the datasheet, you can connect these components in parallel. Is there an in-built current sharing mechanism?

Thanks