Tool/software:
Hello I have designed a buck converter around the ic lm5085.
Vin is 22-57V and Vout is set to 21.5V with Rfb1 and Rfb2.
Increasing voltage on Vin increases voltage on Vout.
Vin = 22V Vout = 21.26V
Vin = 24V Vout = 22.17V
Vin = 26V Vout = 23.05V
Vin = 28V Vout = 23.83V
Vin = 30V Vout = 24.55V
Layout:
I have tried manually increasing Rt with other resistor to lower the frequency in steps from 380khz to 250khz, 200 khz and 180 khz without removing the issue.
Adjusting Rfb1 and Rfb2 relationship to regulate to 10V instead, seems to improve the performance.
To Vout is attached 22 Ohm power resistor to have around 1A draw during testing.
Output has clean output voltage at all measurements
Output from Source on pmos (sorry for screenshots):
24Vin vs 30V vin:
It seems the frequency is changing with Vin?
Worth noting: I messed up footprint of pmos and corrected this manually on development board.
pgate is manually soldered to lm5085 with short copper wire. <1cm