Other Parts Discussed in Thread: TPS631012, USB2ANY,
Tool/software:
I am trying to connect to the TPS631012 EVM board using the USB2ANY module like the instructions setup suggest. The Problem that i am running into is that after the firmware update from the GUI, I am still getting an error saying that It connected to the USB2ANY but could not connect to the TPS631012 on I2c @ 0x2a. I am a bit stuck since I am not seeing any external power being supplied to the EVM from an outside source so I assume that it should be able to connect as is.
After rereading the User Manual I noticed the Enable Jumper Pin but still having the same issue where the USB2ANY board is not connecting to the TPS631012EVM. I assed a 3.3V power supply voltage but the output voltage is still 0V. So I assume I have to program the output voltage but I can't connect to the GUI.
Thank you for your time,
Aaron Porter