Tool/software:
Hello, expert.
I have read other posts about the current accuracy of TPS92520 on the forum.
QA:I would like to consult again about the current accuracy problem of TPS92520:
For 16:1, it refers to ILED_REF_DACx, 1023:63=16:1, is this understanding correct;
QB:For the content of the manual: ANALOG ADJUST SETTING AND CURRENT SENSE AMPLIFIER (CSPx, CSNx);
I understand it like this: For different values of ILED_REF_DACx, the final LED current accuracy is different. The larger the value of ILED_REF_DACx, the higher the accuracy of the LED. Is this understanding correct?
① When ILED_REF_DACx = 1023, the range of V(CSPx-CSNx) is 167.5mV, 173.0mV, 178.5mV, and the LED current accuracy is -3.18%~+3.17%;
② When ILED_REF_DACx = 512, the range of V(CSPx-CSNx) is 83mV, 88.5mV, 94mV, and the LED current accuracy is -6.21%~+6.21%;
③ When ILED_REF_DACx = 63, the range of V(CSPx-CSNx) is 6.5mV, 12.5mV, 18.5mV, and the LED current accuracy is -52%~+48%;
Because our driver needs to match different LED loads, under the condition of not changing the hardware, the current error will be very large in the case of small current. Is there any detailed parameter for the LED current range corresponding to different ILED_REF_DACx values? Thank you.