Tool/software:
Hi,
I have a couple of questions:
1. To program the PD controller, the GUI for the TPS26744E-Q1 seems the way to go, is it possible to program the controller without that GUI?
2. This question may show my ignorance on the subject, but is it possible to control a non-TI PMBus DC-DC regulator with the TPS26744E-Q1 via I2C (PMBus)? This relates to the first question in that I imagine this requires custom firmware that cannot be done via the GUI?
The idea is to simply change the regulator output based on what USB PD negotiation occurs, the issue is that the desired DC-DC regulator is not a TI part, but has a I2C slave port for the purpose of control and configuration, which would ideally be tied to the I2C2 port of the TPS26744E-Q1.
Thank you for any help and excuse my naiveness on the topic, let me know if more info is needed to help. Thank you!