Tool/software:
I am using UCC287506 for 36W Flyback power supply,
2 outputs are: 12V power output for fan and 14V output for light load peripheral. with an auxiliary coil of 21V to power the UCC28750 IC.
When I experimented by running with 155V power supply for the power circuit and 24V auxiliary power supply for the IC using adapter. My 12V coil is always stable. However, when I look at the switching frequency (Green channel), the switching frequency is only about 1.3kHz. I am not sure where the problem is. Please help me.
- Yellow channel: Feedback voltage
- Green channel: DRV voltage
- Blue channel: 14V voltage
- Red channel: VDD voltage (IC not connected)
I attach schematic below