Tool/software:
We modified the LM25149-Q1 EVM to 12v output voltage
Modified items: connect VCCX to GND, FB to 49.9K to VDDA
Test conditions: Input voltage 24V, output 12V, connect load machine (1A, 3A, 5A) to verify conversion efficiency
Test results: The average conversion efficiency of the three loads is about 90% (the company's internal regulations must be greater than 95%)
How can I adjust the circuit to improve efficiency?
Thank you