Other Parts Discussed in Thread: TPS50601A-SP, TPS7H4104-SEP
Tool/software:
Hi,
This is Dinesh from iWave Global. We are looking for the 3.3V, 5A and 0.8V, 5A Regulator Parts required for our project in space grade applications. So, I need to know the regulators that supports space grade applications and also to know the regulators that supports the temperature range of -55°C ~ 125°C. Kindly share the details with the following specifications.
Regulator 1:
Input Voltage: 5V
Output Voltage: 3.3V
Output Current: 5A
Regulator 2:
Input Voltage: 3.3V
Output Voltage: 0.8V
Output Current: 5A
Regards,
Dinesh