Other Parts Discussed in Thread: LM5105, LM2103
Tool/software:
Hi,
I am looking for a 100V bus half bridge gate driver with dual inputs and LS input should be inverted. I mean LS out should be high when its input is low, while HS output should be high for high input. Please do not suggest to add a not gate or transitor based inverter at the front end. I want the solution in the gate driver itself. peak current rating of the gate driver should be more than 2A.