Other Parts Discussed in Thread: TPS62869
Tool/software:
Hi Sir
I have a few questions regarding the TPS62868 and TPS62869:
-
Do they have the same I²C address?
-
Do these two devices have a chip ID register? If so, is it the same for both?
-
Are there any differences in their register maps?
Background Note:
Our DSP vendor recommends using the TPS62868 for DVS with their DSP(Power IC's I2C will directly connect to DSP). However, I'm not sure if I can replace it with the TPS62869 without issues. This is because the DSP vendor might be hardcoded to control power ICs with specific I²C addresses or register settings.
If the TPS62868 and TPS62869 have identical I²C addresses, register maps, and chip IDs (if applicable), then perhaps they are interchangeable.