Tool/software:
Thanks for releasing V1.1.0 Quickstart Calculator spreadsheet and fixing the issue with the RCOMP calculation. It appears that the datasheet EQ 48 needs updating also.
For calculating Ccomp , the datasheet suggests using "twice the Load Pole Frequency" (Equation 49), The document "Under the Hood of a Multiphase Synchronous Rectified Boost Converter" suggests using Fcross/10 ( Equations 39 and 40), and it appears the Quickstart Calculator uses the actual Power Pole frequency.
Out of the three options, which is the best choice?