This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14203: VFB out of specifications

Part Number: LMR14203

Tool/software:

Hello,

I have an issue concerning LMR14203. 

I'm converting 24V to 12V using R1 = 14.7K and R2 = 1K. On one board, I mesured 12V as expected but on another one I obtained 12.5V which is out of specifications.

After investigations, I saw that the VFB on the board which is not working is equals to 0.815V which is out of the specifications (0.747 - 0.782).

I replaced the component on the board with the one from the working one and it's working with a measuring VFB = 0.762V.

When I compared the two marking I can see that the text font if different. Could you confirm they are both valid components from TI and how is it possible to have such a gap ? 

Thank you in advance. 

Best regards,

Gaëtan Lavoué