Tool/software:
Dears
Two power boards were designed using TPS659411 to supply power to the DSP core, BUCK1+BUCK2+BUCK3+BUCK4. Board A uses a 12 layer PCB design with capacitors placed on the bottom layer, while board B uses a 4-layer PCB design with capacitors placed on the top layer. The maximum load of board A can only reach 5.3A, and the maximum load of board B is 10A. With the same schematic, the IC uses default configuration parameters without modification. May I ask if the problem with board A is related to PCB design? Could you please provide some advice?
Two power boards were designed using TPS659411 to supply power to the DSP core, BUCK1+BUCK2+BUCK3+BUCK4. Board A uses a 12 layer PCB design with capacitors placed on the bottom layer, while board B uses a 4-layer PCB design with capacitors placed on the top layer. The maximum load of board A can only reach 5.3A, and the maximum load of board B is 10A. With the same schematic, the IC uses default configuration parameters without modification. May I ask if the problem with board A is related to PCB design? Could you please provide some advice?