This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27211: The parameter issue of the chip

Part Number: UCC27211
Other Parts Discussed in Thread: LMG1210,

Tool/software:

Could you please take a look at what the parameters of the UCC27211 and LMG1210 marked in red circles are? We didn't find it.

  • Hey,

    Thank you for reaching out to TI with your questions regarding the UCC27211 and the LMG1210.

    I do not see any parameters marked in red circles. Is there supposed to be an image attached here?

    Thank you,

    William Moore

  • The pictures have been added. Please help take another look. Thank you!

  • Hey,

    The output stage pullup and pulldown resistances for the devices are not directly specified in the datasheet but can be derived using V=IR and the following specs.

    UCC27211 datasheet spec:

    For example, R_LOL can be derived from V_LOL = 0.07V typical and  I_LO = 100mA to get R_LOL typical = 0.7 Ohms under this operating condition.

    Here is the datasheet spec for the LMG1210 also:

    Let me know if there are any questions.

    Thank you,

    William Moore