Tool/software:
I would like to design a battery charger and I would like to have the following features:
1. Parallel connection of DC to DC converters of different power rating
2. Charger voltage should be varied from 21 V to 29 V
3. Charging current must be able to share as per the capacity of the DC- DC module
4. One selected unit to act as leader module so that it can act as the charging controller ( CC and CV Operation).
Please suggest how these features can be added by using UCC39002.
Thanks,
-Mani