Other Parts Discussed in Thread: LM5171
Tool/software:
Hi,
I am designing a 2-phase bidirectional buck-boost converter with a LM5171-Q1. Specification provided below:
Vin=8V
Vout=12V
Iout=360A
Considering efficiency of 90%, calculated Input current is 600A. Ie inductor current per phase will be 300A. Will LM5171-Q1 support this high current application with 2-phase? Is there any maximum current or power limitation for LM5171-Q1?
Regards
ARCHIN N BABU