Tool/software:
Hi Expert,
Have a nice day! I have question need BU team’s support:
For LP8764-Q1, it’s max Iout of each BUCK is 5A:
Support need:
Could BU team help to test the performance of this device on full load operation? Such as the thermal data, Vout ripple, etc,.
The application conditions:
Vin=5V, Vout=3.3V, Io =5A for each channel, total 20A.
(If you already have test data on other conditions, you could also reply to me as reference. )
Best Regards,
Leo Ma