Other Parts Discussed in Thread: BQ25792, BQ25798, TPS25751, TPS25730, BQ76922
Tool/software:
Hi,
We have 12V battery that needs to be charged via USB-C PD. Our aim is to use simple and cheaper battery charging chip that also works with PD controller TPS25730SRSMR. I came up with many options like BQ24179, BQ25792 and other too but please suggested the best suitable option.
I have another question that for these chargers is it must to connect USB data lines to the Charging IC? I am asking this as our MCU (ESP-32) in our case needs to boot/program via USB so if the charging IC needs the USB-C data pins to be connected then we will not be able to use the USB datelines for MCU debug/program.
Thanks and regards,
Muhammad Awais