This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq51013EVM-725 startup fail

Other Parts Discussed in Thread: BQ500110EVM-688

I have the bqTESLA kit,  and it has started periodically failing to start up.

when i place the receiver on the tx pad (bq500110EVM-688), it struggles to start up.

Scoping the PWM output shows the pwm starting up, reducing frequency, then stopping

  This repeats slightly quicker than once per second.

  Sometimes this repeats for 20-40 seconds, then settles. Other times it never settles and continously repeats this.

  Have tried different loads - doesnt seem to affect it.  sometimes very slightly lifting the receiver up from the pad helps.

  I have the earlier receiver bq25045evm-687 which never shows the same problem

Also, the red and green lights blink together - it is led mode 4, and the table doesn't mention both blinking together which is strange.  Unless they are not actually blinking, but going from both on (standby) to a 'startup mode' then failing so going to standby?

Any ideas as what is wrong?

cheers,

Michael.