Tool/software:
1. Battery voltage = 2.9~3.1 V
2. Battery voltage = 1.8~2.9V
3. Battery voltage = lower than 1.8V
4. Battery voltage = 0V
5. Battery voltage = Floating (Open)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
1. Battery voltage = 2.9~3.1 V
2. Battery voltage = 1.8~2.9V
3. Battery voltage = lower than 1.8V
4. Battery voltage = 0V
5. Battery voltage = Floating (Open)
Hi Shawn
The system application is if the battery pack has 0V charge function of PCM, could you share the charge/discharge behavior with us?
The BQ25170J has four charge phases:
1.) Trickle Charge, Vbat 0V to 2.2V and current limited to 16mA
2.) Pre-Charge, Vbat 2.2V to 2.8V and current is 20% of ISET (Fast Charge)
3.) Fast-Charge (CC), Vbat 2.8V to VSET and current is ISET
4.) Taper-Charge (CV), Vbat VSET and current is below ISET and decreasing.
During Discharge:
1.) When battery voltage 100mV below VSET Recharge will start