Tool/software:
Hello,
we are using CYPD4226-40LQXIT in conjunction with MUX TUSB1046AI-DCI. The Host CPU is Xeon D-2796TE . The circuit works and we are now performing a low temperature testing. At temperatures below 0 deg C, there are no issues if we power up the part and then lower the temperature. However, if we perform a cold start at negative temperatures then USB doesn't work. The display sometimes work or sometimes it doesn't.
Do the equalization values vary with temperature? Is that something we need to recalibrate? At low temperatures does it need lower gain or higher gain?
Is there anything else you can suggest to debug or troubleshoot?
Thanks,
Divakar