This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2113A: TPS2113ADRB Io setting R value max=?

Part Number: TPS2113A


Tool/software:

Hi.

The TPS2113ADRB datasheet says ABSOLUTE MAXIMUM RATING Io=MAX 2.5A, RECOMMENDED OPERATING CONDITION Io=MAX 2.0A.

Can I set it to 2.5A with R_ILIM=200ohm and use it?

Thanks~