This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62869: default output

Part Number: TPS62869


Tool/software:

Hi Sir,

can the voltage of TPS628690ARQY be set to 0.72v when it is first started?

  • Hello Ryan,

    thanks for reaching out in E2E.

    No, the voltage of the TPS628690ARQY cannot be set to 0.72V when it is first started using the VSET/VID pin. The available start-up voltages for this specific device range from 0.200V to 0.575V, depending on the external resistor connected to the VSET/VID pin.
    However, after the soft start-up period, the output voltage can be changed to 0.72V using the I2C interface by writing to the VOUT Registers.

    Best regards,

    Andreas.