This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM70660: Layout Questions

Part Number: LM70660

Tool/software:

Hi Team,

Customer use LM70660 with below layout questions, could you please help check them? Thanks.

  1. Currently, they connected AGND with PGND, is it correct?
  2. 17-pin AGND and 30-pin PGND are connected together inside the IC, so whether there is a need to connect them together in the external circuit? They are connected together on the EVM, could you please help explain the reason here?
  3. Whether this device must uses shunt + amplifier to do current sensing?

BRs,

Francis