Tool/software:
Hello everyone,
I'm working on designing a PCB using the LMQ644A2-Q1 step-down converter to get a 12V output at 12A from a 28V DC input. I based my design on the LMQ644A2 Quickstart Tool I previously used for a similar project.
Could anyone please review my schematic and advise if any modifications are necessary? I would appreciate any feedback or suggestions.
Additionally, I plan to operate the converter over a wider input voltage range of 12V to 36V while maintaining the same 12V output at 12A. Is it feasible to adjust the input voltage within this range without changing other components like resistors, capacitors, or inductors?
I've attached my schematic for reference.
Thanks in advance for your help!