Other Parts Discussed in Thread: TPS65131EVM-839, TIDA-00689, TPS65131,
Tool/software:
Hi TI Expert!
We have implemented a 5V to +/-15 supply in one of our designs. The load is light, below 20mA but hopefully below 10mA.
The following information was used as a foundation for the design, i.e. component selection and layout: datasheet typical application (4.7uH), eval. board design TIDA-00689 (this is our main reference, we also need a compact design, 10uH), eval. board design TPS65131EVM-839 (for TPS65131, 4.7uH)
L1, L3 is Wurth 744031006 (6.8uH). It is a compromize between 4.7uH and 10uH in an attempt to minimize ripple. The inductor family Wurth 744031XXX is recommended in the datasheet.
Our issue is the large output ripple at light loads (i.e. no load, 3mA or 10mA) when enabling the power save mode (PSP, PSN high). Efficiency and low ripple is prioritized because the power supply will be used in a battery powered sensor system.
Especially the +15V ripple is too high (>150mV p-p, not uniform, see below) and it also generates a 200 mV p-p ripple at the 5V input supply even when supplied from a linear lab supply.
Figure 8-11 in the datasheet shows a 50mV pp VPOS ripple with power save mode on and 20mA load.
The general VPOS ripple in our measurement is similar but sometimes TPS65131-Q1 seems skipping controlling the output voltage for some time which generates a larger p-p ripple. Also the voltage increases suddenly, this doesn't align with Figure 8-11. With power-save mode OFF, the ripple looks more normal, see below.
The 5V supply is generated by an isolated DC/DC converter in the complete design. The large current ripple at the input of the TPS65131-Q1 circuit interferes with the isolated DC/DC output voltage control which is another issue.
Schematic diagram:
+15V ripple at 3mA load, power-save mode ON (discard ch2)
+15V ripple at 8mA load, power-save mode ON (discard ch2)
+5V ripple, power-save mode ON (discard ch2)
+15V ripple at 10mA (?) load, power-save mode OFF (discard ch2)
+5V ripple, power-save mode OFF (discard ch2)