Other Parts Discussed in Thread: LM5118
Tool/software:
Hello!
I have a setup with the following parameters:
| Vout | Vin | Imax | 
| 8.9V | 9-24V | 2A | 
All component values have been verified with the LM5118 Quick Start Component Calculator to ensure plenty of phase margin in both Buck and Buck-Boost mode.
The regulator performs just fine for input voltages above 13V and voltages below 11V. 
However, for a narrow region of input voltages between 11.5V and 12.5V (with a slight hysteresis), I am observing a large ripple or oscillation on the output voltage for load currents between ~100mA and 400mA.
The frequency of this observed signal increases with load current until it disappears entirely at around ~400mA.

There seems to be some sort of oscillation in the transition region from buck to buck/boost mode.

Is this a stability issue or related to the board layout?