Hi,
I am performing some test on the BQ77PL900 EVM. Most of the functionality are working fine but when I connect the charger to the EVM I notice that the charge FET is always off, blocking the charge current, even if the CHG (BIT7 of the STATUS register) is set to 1, indicating that the FET should be ON.
If I bypass the charge FET by shorting DRAIN to SOURCE, then the EVM works fine, charging the battery pack, detecting OV and entering in balancing mode, but since the FET is bypassed I need to manually disconnect the charger in order to really balance the cells.
Thanks for your help.