This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Request for design support

Part Number: BQ34Z100-R2

Tool/software:

We have decided to use BQ34Z100-R2 in one of our application. The system is completely working on the battery. This device is used to monitor the battery of the system.

The battery we are planning to use is Ni-Cd. 9.6V, 9800mAh. That mean 8 cells in series.

We are not using the LED indications as in the reference circuits. We would like to use the I2C communication to the controller in the system. 

Please share a reference circuit which can be used for this application with proper explanations.

email - svarghese@oes-inc.com