Part Number: BQ25672EVM
Other Parts Discussed in Thread: BQ25798
Tool/software:
Hello,
I am testing the this BQ25672EVM kit:
I have connected a 4V battery to battery input, I have a solar panel connected to VIN2. All registers are default.
When voltage from solarpanel > 3.6V charging starts as it should but,
when voltage from solarpanel is between 2.5V and 3.6V current drawn from battery is around 400uA. How can I get this down to 20uA?
When solarpanel voltage is below 2.5V current drawn from battery is around 20uA.
Edited: Low current is 20uA not 2uA