Other Parts Discussed in Thread: TPS25751, BQ25758
Tool/software:
Hi Team,
We use BQ25756 in one of 10-Cell Bidirectional Battery charger project. TPS25751 support 5V/9V DFP for BQ25756.
We use our TPS25751 i2cm to control the BQ25756, when in DFP, TPS25751 will send the i2c command to BQ, and generate the PDO voltage value.
Stable load mode : 5.15V / 0A , 4.40V / 3A ; 9.30V / 0A , 8.55V / 3A
Dynamic load mode: 5.40V / 0A , 4.15V / 3A ; 9.55V / 0A , 8.20V / 3A (Over shoot / Under shoot)
1. How to compensate the BQ25756 DFP voltage drop ?
2. How to avoid the BQ25756 DFP voltage over shoot / under shoot ?
Thanks and Regards,
Giedi Wang