Tool/software:
Hi,
I'm using the BQ25798 with shipfets installed.
I place the system in backup mode, so only the battery is present, only the battery is powering the system.
In that situation, I plan to shutdown the system to minimize any Iq from BAT. (It is for storage, we will only re-start placing the adapter on again).
My question (1) is: in that scenario, what is the difference between ship mode vs shutdown mode? The only power source is a battery.
And the question 2: with shipfet installed, where is the correct point of connection of the pin BATP? (direct to BAT+ or BAT IC pins?).
Thanks in advance.
REGARDS