Tool/software:
Hi,
I have designed a PCB using UCC256601 as the LLC controller. It is designed to deliver 750W output power at 48V. The output is not steady, it seems to have a 1s ripple, probably indicating some fault. The output looks like this:

The LS gate output is as follows. It has some sort of packets of switching pulses. However, it does not look like the 400Hz burst mode packets.

I have also probed the voltage across ISNS. (Green - ISNS, Yellow - Output)

The 1 second aligns with the idle time after a fault, however I couldn't locate it. It'd be great if I could get some assistance with debugging the fault.





The current seems to be affected by the probe, I suspect it to be the capacitance.