This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25630: D+/D- pins alternate function

Part Number: BQ25630

Tool/software:

Hi

The BQ25630 Evaluation Module describes that D+/D- pins can have different functions. Is the information correct? How can we enable the ILIM and STAT functions on D+/D- pins?
BR
Gilberto
  • Hi Gilberto,

    Please allow me to clarify. The BQ25630 IC only has D+/D- functionality for these 2 pins. There is no method to enable other functions. 

    In the future we have plans to release an alternate part from this IC family, which will have ILIM and STAT functions instead of D+/D-, hence why there is reference to these alternate functions on the EVM board. I do not have a timeline for when this part is set to release at this time. 

    Best Regards,

    Garrett