This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5157: Asking guidance looking for TI dual DC supply solution with wide input range, +/-15V @ 33mA

Part Number: LM5157
Other Parts Discussed in Thread: LM5155, , LM5175

Tool/software:

Hi Experts,

Would like to ask guidance from PL to offer suitable TI device for dual DC/DC outputs with the following requirements:

Vin range: 4.5V to 28V
Outputs: +/-15 at 33mA

This can be isolated or non-isolated. Would have to be a buck-boost, SEPIC, or flyback capable of running on the full input voltage range (i.e lm5157, lm5155 and etc). We wanted this to run off a 5v, 12v, or 24v supply, can limit it to a 12v and 24v supply instead. Could also boost up to over 28 volts and couple the inductor with + and - outputs.

Any solution to offer is highly appreciated.

Thank you.

Regards,
Archie A.