Tool/software:
When using DDSG, there is still a voltage of 0.6V when a low level is required. After BQ7652 was powered off and then back on, DDSG returned to normal. The internal configuration's pull-up source is REG1, configured at 3.3V.
At DDSG 0.6V, it was also found that the temperature of the external voltage reducing transistor for REG1 was very high. After resetting BQ76952, it also returned to normal.
At DDSG 0.6V,
At the same time, it was found that the collected values of NTC would fluctuate between 25/37 ℃.
Can you help me clarify what caused this situation? How has it been handled?